CADDataAvailability
CAD data availability
New endpoint available: CadDataAvailability
Introduction
The CADDataAvailability provides you with the list of CAD data. For the couple catalog/part number provided, you can know if it is available, if a 3D view can be requested, and which CAD formats can be downloaded.
API Key
This web service requires an API Key. Please use the form to request your API Key.
Description
The API returns if the part number exists on TraceParts. In this case, will be returned the 3D viewer capability and the list of CADFormatID with their labels.
Building a URL
The CADDataAvailability API request takes the following form:
https://ws.tracepartsonline.net/tpowebservices/CADdataAvailability?parameters
Parameters
Certain parameters are required while others are optional. As it is standard in URLs, all parameters are separated using the ampersand (&) character. The list of parameters and their possible values are enumerated below.
Required parameters
Parameter Name | Data type | Default value | Description |
---|---|---|---|
ApiKey | string | none | Code calling an API to track and control how the API is used |
Format | string | none | Answer file type (xml, json) |
PartID* | string | none | PartID given by the SynchronizationData API |
ClassificationID** | string | none | ClassificationId given by the CatalogsList API |
PartNumber** | string | none | Part Number as it is exactly written in the TraceParts database |
Language | string | en | LanguageID given by the LanguagesList API |
Optional parameters
Parameter Name | Data type | Default value | Description |
---|---|---|---|
UserEmail | string | none | User email / User ID |
ActiveJsonLight | boolean | 0 | Enables the light version when json is the answer file type |
SelectionPath* | string | none | SelectionPath given by the SynchronizationData API |
*Both parameters (PartID and SelectionPath) have to be used together. In this case, the couple “ClassificationID” and “PartNumber” is not to use.
** Both parameters (ClassificationID and PartNumber) have to be used together. In this case, the couple “PartID” and “SelectionPath” is not to use.
Example of CADDataAvailability API
The request below returns the CAD data availability as an xml file for the part number 43900011 from the catalog ASCO Numatics.
PartID and SelectionPath:
https://ws.tracepartsonline.net/tpowebservices/CADdataAvailability?PartID=10-17102002-114249&SelectionPath=1|1|1|1|&Language=en&Format=xml&ApiKey={ApiKey}
PartNumber and ClassificationID:
https://ws.tracepartsonline.net/tpowebservices/CADdataAvailability?PartNumber=43900011&ClassificationID=ASCO_JOUCOMATIC&Language=en&Format=xml&ApiKey={ApiKey}
By changing the Format and adding the ActiveJsonLight, CADDataAvailability returns the availability as a light Json file.
https://ws.tracepartsonline.net/tpowebservices/CADdataAvailability?PartID=10-17102002-114249&SelectionPath=1|1|1|1|&Language=en&Format=json&ActiveJsonLight=1&ApiKey={ApiKey}
CADDataAvailability responses
CADDataAvailability responses are returned in the format indicated by the Format parameter within the URL request’s path.
JSON Output
A sample HTTP request is shown below, displaying a sample of the available CAD formats, the Part Number and 3D viewer availabilities.
{
"partNumberAvailability":
{
"partNumber":"43900011",
"availability":true
},
"viewerAvailability":true,
"cadFormatList":
[{
"cadFormatId":33,
"cadFormatName":"3D XML"
},
{
"cadFormatId":2,
"cadFormatName":"Acis 6.3"
},
{
"cadFormatId":11,
"cadFormatName":"AutoCAD (DWG 13) - 2D"
},
{
"cadFormatId":48,
"cadFormatName":"ZW3D"
}]
}
XML Output
Same example as above.
<WsCADdataAvailability>
<CADFormatList>
<WsCADFormat>
<CADFormatId>33</CADFormatId>
<CADFormatName>3D XML</CADFormatName>
</WsCADFormat>
<WsCADFormat>
<CADFormatId>2</CADFormatId>
<CADFormatName>Acis 6.3</CADFormatName>
</WsCADFormat>
<WsCADFormat>
<CADFormatId>11</CADFormatId>
<CADFormatName>AutoCAD (DWG 13) - 2D</CADFormatName>
</WsCADFormat>
<WsCADFormat>
<CADFormatId>48</CADFormatId>
<CADFormatName>ZW3D</CADFormatName>
</WsCADFormat>
</CADFormatList>
<PartNumberAvailability>
<Availability>true</Availability>
<PartNumber>43900011</PartNumber>
</PartNumberAvailability>
<ViewerAvailability>true</ViewerAvailability>
</WsCADdataAvailability>
CADDataAvailability response elements
CADDataAvailability responses contain five elements:
- “PartNumber”: part number without any special characters, ignored by TraceParts for the search feature (” “,”-“,”.”,”/”,”+”).
- “Availability”: true or false if the PartNumber is available or not on the TraceParts database.
- “ViewerAvailability”: true or false if you can use the 3D viewer API.
- “CADFormatId”: defined by TraceParts, usable with other APIs.
- “CADFormatName”: label of the CAD format, written in the current language.
- “DeliveryMethod”: way of CAD file delivering. 1: URL to the file | 2: URL to a web page for the selection of the file | 3: Command for Fusion 360 to open the file in the CAD software.
Developer support
Please contact us for any problem, question or comment related to this content integration.
Last updated January 28, 2016
Updated 10 days ago