Découvrez les fournisseurs de composants hydrauliques déjà présents sur traceparts.com
La publication de catalogue de produits sur la plateforme d’ingénierie TraceParts, génère des téléchargements de modèles CAO.
C’est pourquoi les fournisseurs de composants hydrauliques ci-dessous ont choisi la plateforme de contenu CAO TraceParts pour publier une partie ou la totalité de leur gamme de composants hydrauliques.
Dès qu’un modèle CAO est téléchargé, les fabricants et distributeurs reçoivent ainsi des informations clés sur le contact qui a utilisé leurs composants, notamment son adresse email, sa société, le type d’industrie, et d’autres informations liées au parcours utilisateur.
Cliquez sur un des logos pour accéder au catalogue.


afy
Nous distribuons des raccords de qualité répondant aux normes européennes
Andrex VALVE GROUP
ANDREX VALVE GROUP has started its activity with the production of metal elements made from acid resistant steel. The key products has been the supports for the pipelines which have been installed all over the world by the reputable international company
ANR Engineering
ANR manufactures hydraulic cylinders, special components for hydraulic cylinder, transmission and engine transmission elements, aircraft special spare parts, components for garbage trucks and sweepers.
ASSFALG Qualitätshydraulik
Hydraulic cylinders and accessories
Astore
Manufacturer of Manual valves, Compression fittings, Compression fittings, PVC pressure fittings
ATEC-CYL S.A.
Established since 1994 in the Swiss Jurassic Arc, the cradle of watchmaking and microtechnology, Atec-Cyl SA is specialized in hydro-pneumatic solutions and products as well as mechanical subcontracting.
Atos
We internally develop all of our expertise in electrohydraulics, foundry, fluidics, mechanics and electronics.
AVIT - Hochdruckrohrtechnik
High Pressure Tubing Technique, Wlding Screw Connections
Bavaria Fluid Systems GmbH
Bavaria Fluid Systems GmbH develops and manufactures customer-specific valve and pump solutions based on existing valves and pumps for the (high-tech) industry.
BEE
Manufacturer of Ball Valves and Safety Valves
BERARMA
The Italian leading manufacturer of variable displacement vane pumps up to 250 bar, since 1963.
BOSCH REXROTH - Hydraulics
Hydraulics
CAMAN
We are now a major supplier of valves for the gas, petrochemical and general industries. Caman has one of Australia's most complete range of valving products. No matter what the application, we have the solution. Our valve sales team are among the most experienced in the country.
CEJN
Quick connect couplings and nipples
CEPEX
Fluid handling experts
Cross Manufacturing, Inc.
Manufacturer of hydraulic components including cylinders, valves, gear pumps, motors, accumulators, filters, valves and fittings. Suitable for agricultural, construction, material handling, marine, mining, forestry and industrial applications. Made in the USA.
CSF Inox S.p.A.
CSF Inox SpA produces over 600 different kinds of pumps for the food, pharmaceutical and beverage industries
donadon
Manufacturer of safety devices since 1950
EDH
Le spécialiste du réservoir, de l'accessoire hydraulique et de la mise en propreté des fluides.
ENERPAC
High-force tools & equipment used in industrial markets
Eurobinox
Fabricant de robinetterie hygiénique et aseptique dans les domaines de l’Agroalimentaire, Cosmétique Pharma, Biotechnologie, vinicole. Notre service négoce distribue accessoires, tubes, raccords, tés, coudes et autres aux normes SMS, DIN, RJT, ISS, ISO.
FG INOX
The global solution for your needs in stainless steel
FILTON
Specialise in the field of fluid transfer engineering and manufacture air breather filters, and rotary and swivel joints
FIP
Manufacturer of U-PVC, C-PVC, PP-H, PVDF fittings and valves
FKB GmbH
Befestigungstechnik
HANDA
Handa Machinery is a professional manufacturer and exporter of hydraulic cylinders and power units. Handa currently covers 13,000 square meters with modern workshops and cutting edge equipment. The 6S and E R P management systems are rigidly implemented throughout the company. Handa is I S O 9 0 0 1 and C E certified. Handa cylinders have been widely used in machinery industry, agricultural equipment, trailers, excavators and other fields. We can supply all models of tie rod, welded, single & double acting cylinders. We can also customize hydraulic cylinders to meet customers' requirements on mounting styles, pressure ratings, sizes and configurations. At Handa, standardization is tirelessly implemented throughout the entire process. At Sales Department, all customers’ profiles & requirements are documented through E R P system, to help track all aspects of each order. At R & D Department and Engineering Department, P L M system is implemented to process drawings and technical data. At Sourcing Department, stable raw material suppliers are regularly evaluated, to keep the cost down. In the Production Department, Lean Production Management and M E S system are adapted. The Q C Department are equipped with precision instrument & machinery, standard process management, 100 % testing capacity & trace -ability. One of our core values is to partner with customers and provide world- class customer services. With “Easy to do business with” attitude, Handa is your trusted, supportive, and most reliable partner.
Hengli Hydraulic
Hengli has developed China’s largest, most influential hydraulics manufacturer with the most complete product lines and has been providing global customers with safer, more efficient and rationally-designed hydraulic transmission and control solutions
Hositrad Holland B.V
The Hositrad Holland and the Hositrad Deutschland team has more than 50 years experience in vacuum and cryogenic technology. We have capabilities covering all areas starting from a standard flange up to designing a complete system, manufacturing or repair and after sales service of your vacuum equipment. We are a supplier of basic flanges, valves, electrical feedthroughs, edge welded bellows, manipulators, ion pumps, vacuum chambers up to a complete sputtering. Most of these items we supply from stock.
HUADE Hydraulic
One of the most important hydraulic enterprises and the biggest production bases of hydraulic components and power units in China.
HYDROBLOCK SRL
Hydroblock manufactures locking systems for machine tools capable of guaranteeing functionality, safety and reliability in extreme working conditions.
Hydropa
Hydraulic Cylinders
IMP PUMPS
IMP Pumps d.o.o. is Slovenian manufacturer of pumps and pumping systems located in Komenda in Slovenia. Company designs, develops, manufactures, distributes and maintains pumps and pumping systems.
INOXPA
Manufacturer of pumps
Jiaxing Master Fitting
The Compression, welded, flared fittings and wire-netted, stainless steel braided hose assembly and connector assembly are widely used in all kinds of high, medium and low pressure pipe line systems with oil and gas as media
Jining KERSEN
Registered fund RMB 50 million .Specialized in technology development , manufacturing and selling orbit hydraulic units .The leading products are hydraulic motor and steering control units.
LUKAS Hydraulik GmbH
Germany's finest hydraulics
NUPI
Nupi Industrie Italiane SpA offers a full range of pipes and fittings made of the most modern thermoplastic materials.
OLAER
Manufacturer of basic product in hydraulic equipment
Parker
Motion & Control Technologies
PLAS-FIT
Plas-fit is one of the leaders in the pipe fittings industry. In Israel and around the globe, Plas-fit designs, develops, manufactures and markets top quality fittings and advanced plastic products for a variety of uses in a wide range of industries: Agriculture and Landscaping, Water, Industry, Infrastructure, Communications and Technology.
POLLARD PUMPS
Since 1946, Pollard has designed and produced positive displacement pumps adapted to the specific problems of industrial customers.
Pushfit.se
Connectors and hose for drinking water, vending machines, and beverage equipment
RAFIX
For 6 decades, RAFIX has designed and manufactured in France a catalog of 3000 Quick Couplings. Contract manufacturing covers interface, raw material, dimensions, identification, threading, gasket for Nuclear Energy, Process, Fine Chemicals and Cosmetics.
ROCKY
Manufacturer of valves
ROEMHELD
Manufacturer of hydraulic elements and systems for production engineering
RÖTELMANN
Shut-off and Control Technology
SAB Bremen

SAFI
Thermoplastic valve solutions
SALMSON
Design and manufacture of pumps and pumping systems
SEALCON
Cable Management Solutions
Seals-Shop.com – Trelleborg Sealing Solutions Germany GmbH
Seals-Shop.com – the online shop of Trelleborg Sealing Solutions for the fast purchase of seals. We stock a broad spectrum of hydraulic seals of all kinds, suitable for a wide range of applications, from simple linear systems through to heavy-duty rotation applications.
SH - SIDERFIL HIDRÁULICA
The SIDERFIL HIDRÁULICA is a company retaining the highest technology in the development and manufacture of hydropneumatic accumulator operating since 2001 where it has specialized professionals with extensive industry experience
Shanghai Huatong Valve
Shanghai Hua Tong Valve Co., Ltd. (formerly state-owned enterprise restructuring, founded in 1970), is a set of product development, design, production and sales of specialized high-end valve manufacturing enterprises.
SOFRA-INOX
SOFRA-INOX spécialiste des raccords et pièces détachées en inox pour l'industrie.
Standard Hidráulica
Standard Hidráulica is recognized as one of the leading solutions manufacturers for Connections, systems and regulation, Heating, control and safety, Pipe network and Taps.
Star® Pipe Products
Star Pipe Products is a global manufacturer and supplier for a broad array of iron products, including Ductile Iron Pipe Fittings and Accessories, Joint Restraints, AWWA Grooved Products, and Municipal and Construction Castings.
STAUFF®
Mechanical connection elements
Stransky a Petrzik
Stransky and Petrziz is a Czech manufacturer of pneumatic cylinders and accessories, which in connection with its development enables not only fast and high-quality production of standard pneumatic components, but also special components designed and manufactured according to customer requirements.
Sun Hydraulics
Manufacturer of high performance screw-in hydraulic cartridge valves and manifolds
Swagelok
Fluid system solutions
Tecofi
Manufacturer of industrial valves
TST Tamsan
TST is a manufacturer of quick connection elements, mainly in the form of Quick Release Couplings/ Coupling Systems.
TUPY
A Brazilian foundry, TUPY is present in all continents and is a reference trade mark in the international market of cast iron components
Valworx
Valworx is a leading supplier of actuated valves and accessories. Stainless, brass, PVC, sanitary ball and butterfly valves. Electric, pneumatic and manual actuation.
Victaulic
Today, Victaulic innovative piping systems, technologies and services put people to work faster while increasing safety, ensuring reliability and maximizing efficiency. The company has 15 major manufacturing facilities and 28 branches worldwide with 3,600 employees who speak 43 languages across the globe. With over 1,800 active global patents, Victaulic piping solutions, perfect as welding alternatives, are at work in more than 125 countries across diverse business lines including oil and gas, chemical, mining, power generation, water and wastewater treatment, military and marine, as well as commercial building and fire protection.
WEH Precision Connectors
Quick Couplings for filling applications, leak test, pressure & vacuum tests in hydraulics, pneumatics, gas industry, HVAC-R, automation. High-performance check valves for liquid and gaseous media. Components for CNG refueling and hydrogen refueling (H2).
wilo
Wilo is a premium supplier for the building services, water management and industrial sectors. We make complex technologies user-friendly, simple to operate, energy-efficient and powerful for our customers.