The Newsletter to The TraceParts Design Engineering Community #169

June 2022 – New parts catalogs available on the TraceParts CAD-content platform: Motion Industries, Phoenix Contact, NADELLA, ROSS Controls, SCHWEIZER.

TraceParts Newsletter #169 New components provided from Motion Industries, Phoenix Contact, NADELLA, ROSS Controls, SCHWEIZER

TraceParts

NEW AND UPDATED CATALOGS  | June 2022

Browse any of the catalogs below to speed up your next design project

with manufacturer certified catalogs on TraceParts.com

Motion Industries

Motion Industries

Bearings, mechanical power transmission, electrical and industrial automation, hydraulic and pneumatics…

New Components

  • Airframe Control Ball Bearing, B538FS160
  • Spotting Drill, 087905
  • Jobber Length Drill Bit, 018010

Airframe Control Ball Bearing, B538FS160

Browse Catalog →

ACE’s Industrial Gas Springs for Gentle Movement

The new go-to components for quick & easy locking without the use of tools

One Touch Fasteners provide secure, reliable clamping at the turn of a handle or push of a button. Quickly lock and unlock fixture plates, covers, machine components and more, with no time wasted tightening old-school screws and nuts. Quarter turn, button locking, pin holding and magnetic types are available, as well as full stainless steel versions. Ideal for quick changeover applications.

SEE THEM IN ACTION

Phoenix Contact

Phoenix Contact

Phoenix Contact is a leading developer and manufacturer of industrial electrical and electronic technology.

New Components

  • C-RCI 10/M6 Ring cable lug
  • PSR-ESS-M2-H110-2000-A
  • SC-LR SP
Browse Catalog →

C-RCI 10/M6 Ring cable lug

NADELLA

NADELLA

The Specialist for Motion Technology

New Components

  • NA.. – With inner ring
  • Telescopic Rail, NTS28-26H Hardened Full extension
  • KR..EE – Concentric stud

NA.. - With inner ring

Browse Catalog →

ROSS Controls

ROSS Controls

Manufacturer of pneumatic valves, controls systems, and safety products for the fluid power industry.

New Components

  • Energy Isolation Safety Lockout LOX® Valve
  • Cam Valve, 2-way Roller, Port Size 1/4″ NPT
  • Manual Lockout LOX® Valve, 15 Series, Port size 3/4″ NPT
Browse Catalog →

Energy Isolation Safety Lockout LOX® Valve

SCHWEIZER

SCHWEIZER

Springs and Accessories

New Components

  • Compression springs – Spring steel
  • Extension springs – Spring steel
  • Compression springs – Stainless steel
Browse Catalog →

Compression springs - Spring steel

ENGINEERING NEWS

with friendly support from EngineeringClicks

Magnetic Bearings – The mechanical engineer’s guide

Magnetic Bearings – The mechanical engineer’s guide

As the name suggests magnetic bearings use magnetic levitation to support the rotating shafts, without directly contacting them, thus there is no friction. As we all know, less friction means less energy wasted and greater overall efficiency. The very first patent relating to the magnetic suspension of rotating elements was submitted in the 1940s. However, the first widespread applications did not occur until the seventies. 

Read More →

Mechanical Designing in the Automotive Industry: A General Outline

Mechanical Designing in the Automotive Industry: A General Outline

While it is easy to find rich, interesting analyses on the way finance companies, law offices and software labs’ inner processes are conducted, little is known about the insides of factories, industrial companies or R&D departments in the mechanical engineering sector. At MDF, we are eager to initiate the public and future mechanical engineers into our domain and give a clearer image of what goes on within our offices.

Read More →

Aerodynamics Basics – Know the fundamentals

Aerodynamics Basics – Know the fundamentals

Have you ever wondered why cars have spoilers or why your hand ‘floats’ when you hang it out the window of a moving car? These mysterious interactions between objects and air have long been studied and are known collectively as aerodynamics. The term aerodynamics comes from two words: aero (air) and dynamics. Dynamics is a branch of mechanics concerned with the motion of a body under the action of forces.

Read More →

facebook

twitter

youtube

linkedin

TraceParts S.A.S.
Parc Eco Normandie
76430 Saint Romain – France

E-Mail: info@traceparts.com
Web: www.traceparts.com
Phone. +33(0)232 794 426

Trade register number: 433 949 625 000 19
VAT. No FR53433949625

You are receiving this newsletter because of your registration with TraceParts.

Our General Terms of Use & Privacy Policy can be found here. Information on our GDPR compliance can be found here

关于作者

Helena Tomic
Helena Tomic

Marketing Specialist, TraceParts