了解哪些 制动器、离合器和联轴器 的供应商已经在 traceparts.com 展示产品
在工程平台 TraceParts 上发布产品目录将带来 CAD 模型的下载。
这就是为什么下列 制动器、离合器和联轴器 供应商选择 TraceParts CAD 内容平台发布其部分或全部 制动器、离合器和联轴器 产品。
当有人下载 CAD 模型时,相关零部件的制造商和/或分销商就会收到使用其零部件的联系人的关键数据,尤其是他(她)的电子邮件地址、公司和行业类型以及与用户旅程有关的其他信息。
点击徽标查看目录。


ALANCO ALAMATIC Ltd.
At Alanco Alamatic we manufacture our own industrial disc brakes (industrial disk brakes), industrial brake discs, safety chucks and tension control equipment.Our diverse range of products are used for converting applications, where the manufactured item is in reel form. Typical products, in reel form, include paper, plastics, plastic film, aluminium foil, textiles, cables and steel. Our industrial disc brakes (industrial disk brakes) can also be used in a wide range of linear applications such as test rigs, conveyors, bridges and tension control systems, in addition to general stopping, or holding duties - for industrial machinery.
BAP
Specialized in design & manufacturing of mechanical transmission equipment.
Belden Universal
High-Performance Universal Joints and Drive Shafts for Standard and Complex Applications
CHENGZHI
Suzhou Chengzhi Precision Machinery Co., Ltd. is founded in 2008, which is a high-tech private enterprise specializing in the production of couplings. It has high-end technical personnel and high-quality work team, it can timely provide customers with perfect product development and after-sales service.
CMD COUPLINGS
Mechanical power transmission
ComInTec S.r.l.
Torque limiters, pneumatic clutches, couplings, adjustable pulleys, motor-slide bases and components for the assembling of automatic machines
CTS
Manufacturer of bearings and special drives
EPIDOR
Empresa especialista lider en la distribución de productos de calidad para la industria
ESCO COUPLINGS N.V
High-quality Couplings manufacturer and Transmission products specialist and distributor, ESCO has been connecting the world for more than 70 years.
GIRARD TRANSMISSIONS
Precision worm gears
GZ LINK
As the manufacturer of shaft coupling and ball screw support unit, We Guangzhou LINK Automation Equipment Co., Ltd focus on development and production of high-quality & precise shaft coupling.
Huco Dynatork
Manufacturer for Couplings and Motors
Imetex
Supplier of components for machines and industrial equipments
ISEL
ISEL is a company name that says it all. Every way we do business is reflected in the name that condenses our concept. Product sales are just a part of what we do because we create exactly what customers are looking for using our imagination, expertise and effort.
KTR
Power transmission
magneta
Manufacturer of electromagnetic clutches and brakes
MAGTROL
Hysteresis brakes and clutches for tension
MAV
Manufacturing keyless locking devices, shrink discs and rigid couplings
mayr power transmission
Drive elements
MEROBEL
EMP Brakes & Clutches (ElectroMagnetic Particles), Web Tension Controllers and Electronics, various sensors and transducers for force and torque control
MIKIPULLEY
Development, manufacturing, and sales of transmission devices
PTP INDUSTRY
Transmission Products : Ensuring the robustness of your installations
R+W
Manufacturer of Line Shafts, Torque Limiters and Shaft Couplings
Rexnord Tollok
Locking assemblies
SEPAC Inc
Manufacturer and designer of brakes and clutches. Serves the military, aerospace and defense, robotics, energy, healthcare/medical, automation and a variety of industrial markets.
Shijiazhuang CAPT
A center for research, development, production and sales of specialized transmission products. Products range from 16 major categories, with more than 45,000 specifications.
SIAM RINGSPANN
Manufacturer of transmission, assembly, clamping and control elements
Sigerist GmbH
Sigerist GmbH is a company based in Switzerland. The company was founded over 150 years ago and is active in sales with technical components. At Sigerist, machine feet, wheels, rollers, lifting rollers and lifting systems are among the most important products in the range. This also includes parts for drive technology, such as shaft couplings, shaft clamping rings and clamping sets. In addition to trading, products are developed and manufactured.
SIT
Couplings, Pulleys, Motor bases and Taper lock bushes ATTENTION CAD DRAWINGS PROVIDE INFORMATION ON GENERIC DIMENSIONS AND DO NOT REPRESENT TECHNICAL FEATURES.
Stemin Breitbach
MECHANICAL POWER TRANSMISSION SOLUTIONS
STÜWE
Clamping Sets, Flanges
SUODA Coupling
Zhenjiang Suoda Coupling Co., Ltd is a professional coupling manufacturer which former is a joint venture set up by Zhenjiang Transmission Co., Ltd and American company.
tector
Transmission and torque control solutions
TURIAN
In year 2014 TURIAN ENG s.r.l. has shipped approximately 12000 Rotary Joints, of which approximately 8000 standard from catalog and balance tailor made. All Rotary Joints are individully packed and then boxed as deemed necessary or according to Customer specifications, when available.
UNICUM
Spécialiste français des composants pour la transmission de puissance dans les domaines : freinages industriels et embrayages, réducteurs, renvois d’angle, vérins mécaniques et électriques, entraînements linéaires, accouplements et limiteurs de couple.