Traceparts

The world of 3D design can be very confusing.  Not only is there a wide range of 3D software from which to choose, but designers must pay close attention to the file formats they select when downloading, sharing and saving their creation.  In this blog, we look at the difference between โ€œneutralโ€ and โ€œnativeโ€ file formats.

 

Neutral Formats

Sharing digital documents has become a relatively easy process, as Portable Document Format (pdf) has become increasingly adopted as a universal standard.  In contrast, when it comes to 3D file formats there is no single โ€œindustry standardโ€.  There are some model formats that are designed to be usable by all, including STEP, IGES, Parasolid and several others.  However, there is no single option that is suitable for all applications.  Despite this, there are advantages to using a neutral format.

Neutral formats are designed to be universal.  One of the advantages of a neutral format is that it allows, in theory at least, the chance to share 3D information between companies and collaborators.  Almost all 3D software platforms enable the importing and exporting of neutral formats.  However, there are pitfalls of sharing 3D design information that need to be considered.

The first aspect that needs to be understood is geometry.  The 3D representation of the solid object is, after all, the primary role of 3D modelling.  In order to be truly universal, the geometry of the model needs to be interpreted accurately by any software that uses it.  Errors can occur, and unfortunately, neither IGES nor STEP can be relied up to provide complete accuracy during the import or export process.  This requires designers to perform additional checks to ensure that the transfer of information is correct. 

The second pitfall to be aware of is integration.  A model is only part of the story, and there needs to be accompanying data that allows the model to become part of a design.  This data includes commercial, technical and supply chain information.  It provides the user with information as varied as the part number of the model, its manufacturer, the material from which it is made, and a host of other details.

Even if a neutral file format can contain this information, each 3D software design system may handle the data differently.  In addition, as design software is increasingly integrated with Product Lifecycle Management (PLM) software as part of the Digital Thread, this data is becoming more important.  There are some new neutral formats, such as STEP AP242, that try to address this issue, but problems may remain unseen, ready to come back and haunt the engineer later.

 

Native Formats

There is an alternative to neutral formats.  Every 3D modelling software platform generates its own file format, optimised for use in its own virtual environment.  This is known as the native file format.

When considering the use of native formats, it is important to remember that the current platforms are so much more than simple drafting tools. These are true computer-aided design platforms, not just a replacement for traditional paper-and-pencil techniques. Modern CAD software provides the designer with a range of tools, from simulation to finite element analysis.

Models created using the native format will conform to all of the softwareโ€™s internal rules, and will contain all of the information needed to take advantage of these complex features.  Native CAD models will allow the use of these features in a way that files like STEP or IGES may not be able to access. And there are even examples when STEP files do not even translate their geometry correctly, forcing designers to spend valuable time checking measurements.

However, the real power behind native formats will become clear when we look at the Digital Thread. As 3D design software is integrated into the PLM framework, only models that are native to the CAD system can take full advantage of the through-life support that PLM software provides.

 

Which to Choose?

The choice between neutral and native file formats is not simple.  For engineers that wish to share their designs with colleagues, neutral file formats may be the only choice.  Under these circumstances, designers must be ready to check the accuracy of the information to make sure their work is not corrupted.

If the designer is downloading models for use in new designs, then native file formats are the best possible choice.  The accuracy that is built into a native file will provide designers with the confidence that they have chosen the right component, and that their design will be able to make full use of PLM software.

ะžะฑ ะฐะฒั‚ะพั€ะต

David Pike
David Pike

David Pike is better known asย Connector Geek. With nearly 30 years of experience in the world of interconnect, David enjoys helping engineers understand more about exciting engineering solutions.

ะ”ั€ัƒะณะธะต ะฟะพะดะพะฑะฝั‹ะต ะฐั€ั‚ะธะบัƒะปั‹

ะงะธั‚ะฐั‚ัŒ ะดะฐะปัŒัˆะต

ะšะพะผะฟะฐะฝะธั Bell-Everman ัƒะฟั€ะพั‰ะฐะตั‚ ะฟั€ะพั†ะตัั ะฟั€ะพะตะบั‚ะธั€ะพะฒะฐะฝะธั ะปะธะฝะตะนะฝะพะณะพ ะธัะฟะพะปะฝะธั‚ะตะปัŒะฝะพะณะพ ะผะตั…ะฐะฝะธะทะผะฐ ะทะฐ ัั‡ะตั‚ ะธัะฟะพะปัŒะทะพะฒะฐะฝะธั ะบะพะฝั„ะธะณัƒั€ะฐั‚ะพั€ะฐ ะกะะŸะ  ะพั‚ TracePartsย ย 

ะ“ะพะปะตั‚ะฐ, ัˆั‚ะฐั‚ ะšะฐะปะธั„ะพั€ะฝะธั, 6 ะ”ะตะบะฐะฑั€ัŒ 2022โ€ฏะณ. โ€” ะšะพะผะฟะฐะฝะธั Bell-Everman Inc. ะพะฑั€ะฐั‚ะธะปะฐััŒ ะบ TraceParts ะดะปั ัะพะทะดะฐะฝะธั ะผะพะดะตะปะตะน ะดะปั ะฐะฒั‚ะพะผะฐั‚ะธะทะธั€ะพะฒะฐะฝะฝะพะณะพ ะฟั€ะพะตะบั‚ะธั€ะพะฒะฐะฝะธั (ะกะะŸะ ) ะดะพัั‚ัƒะฟะฝะพะน ะดะปั ะบะปะธะตะฝั‚ะพะฒ ะปะธะฝะตะนะบะธ ะธะทะดะตะปะธะน...

ะงะธั‚ะฐั‚ัŒ ะดะฐะปัŒัˆะต

Hausmann + Haensgen: ัƒะดะพะฒะปะตั‚ะฒะพั€ะตะฝะฝะพัั‚ัŒ ะบะปะธะตะฝั‚ะพะฒ ะฒ ะดะพะปะณะพัั€ะพั‡ะฝะพะน ะฟะตั€ัะฟะตะบั‚ะธะฒะต ะฑะปะฐะณะพะดะฐั€ั ะฟะฐั€ะฐะผะตั‚ั€ะธั‡ะตัะบะพะผัƒ 3D-ะบะฐั‚ะฐะปะพะณัƒ ะดะตั‚ะฐะปะตะน ะฝะฐ ัะฐะนั‚ะต TraceParts.com

ะšะพะผะฟะฐะฝะธั Hausmann + Haensgen, ะพะดะธะฝ ะธะทย ะฒะตะดัƒั‰ะธั… ั‚ะตั…ะฝะธั‡ะตัะบะธั… ะฟั€ะพะธะทะฒะพะดะธั‚ะตะปะตะน ะธ ะดะธัั‚ั€ะธะฑัŒัŽั‚ะพั€ะพะฒะฒ ะพะฑะปะฐัั‚ะธย ะฟั€ะธะฒะพะดะฝะพะน ะธ ะบะพะฝะฒะตะนะตั€ะฝะพะน ั‚ะตั…ะฝะธะบะธ, ะพะฟัƒะฑะปะธะบะพะฒะฐะปะฐ ะพะฑัˆะธั€ะฝัƒัŽ ั‡ะฐัั‚ัŒ ัะฒะพะตะณะพ ะฐััะพั€ั‚ะธะผะตะฝั‚ะฐ ะฒย 3D-ะบะฐั‚ะฐะปะพะณะต ะฟั€ะพะดัƒะบั†ะธะธ ะฝะฐ ัะฐะนั‚ะต TraceParts.com.ย  ะ—ะฐะถะธะผะฝั‹ะต...

ะงะธั‚ะฐั‚ัŒ ะดะฐะปัŒัˆะต

ะ”ะฐะฝะฝั‹ะต ะกะะŸะ  ั€ะฐะทัŠะตะผะพะฒ ะบะพะผะฟะฐะฝะธะธ Harwin ั‚ะตะฟะตั€ัŒ ะดะพัั‚ัƒะฟะฝั‹ ะฝะฐ TraceParts.comย 

ะšะพะผะฟะฐะฝะธั Harwin โ€“ ะพะดะฝะฐ ะธะท ะฒะตะดัƒั‰ะธั… ัะฟะตั†ะธะฐะปะธัั‚ะพะฒ ะฒ ัั„ะตั€ะต ะฝะฐะดะตะถะฝั‹ั… ะธ ะฒั‹ัะพะบะพะบะฐั‡ะตัั‚ะฒะตะฝะฝั‹ั… ัะพะตะดะธะฝะธั‚ะตะปัŒะฝั‹ั… ัƒัั‚ั€ะพะนัั‚ะฒ โ€“ ัั‚ะฐะปะฐ ะฟะฐั€ั‚ะฝะตั€ะพะผ TraceParts, ั‡ั‚ะพะฑั‹ ะพะฑะตัะฟะตั‡ะธั‚ัŒ ะฑั‹ัั‚ั€ั‹ะน ะธ ะฟั€ะพัั‚ะพะน ะดะพัั‚ัƒะฟ ะบ...