All the signs are pointing towards
digitally enabled factories. All the innovations hitting the industrial B2B
market are designed to simplify processes, ramp up safety and pre-empt any
problems.
According to consultancy Deloitte, only 20%
of manufacturers believe that they are wholly ready to face the new business
models generated by the fourth industrial revolution.
1st trend:
IoT
Manufacturers are making increasing use of
the Internet of Things (IoT), which involves interconnecting standalone devices
within an existing Internet infrastructure.
IoT plays an instrumental role in achieving
various objectives, such as lowering costs, improving efficiency, bolstering
safety and addressing product conformity and innovation requirements.
Forbes
predicts that spending on IoT technologies, apps and solutions will reach $267
billion by 2020. This explosion in spending should be driven by the
manufacturing industry, which will transform and digitally connect its business
processes. You can expect to see greater connectivity in everything, from
workshops through to supply chains, with the aim of helping manufacturers raise
the bar on efficiency and productivity.
2nd trend:
Collaborative robots
The fact that the use of robotic systems is
soaring in industry can be explained by the need to prevent people from
carrying out repetitive and sometimes dangerous tasks.
In 2020, people will be talking about smart
robots, rather than just simple robots!
Production lines are being enhanced with
new machines capable of collaborating with human operators and stepping in when
it comes to certain ergonomically challenging activities that can cause a host
of musculoskeletal disorders (MSDs).
These cobots play an essential part in
minimizing difficult working conditions and increasing performance.
However, the collaborative robot revolution
requires a large array of technologies to ensure safety, modularity and
productivity.
3rd trend:
AI, AR and VR
AI (artificial intelligence), AR (augmented
reality) and VR (virtual reality) are other trending technologies that will
shake up the manufacturing industry in 2020.
In addition to adopting IoT technologies,
manufacturers are setting their sights on smart technologies and artificial
intelligence in a bid to gain a competitive advantage.
Machine learning and smart manufacturing
are already helping manufacturing companies to automate their processes and
improve their efficiency, such as in terms of quality control and maintenance.
For example, VR can be used to make quick
tweaks and additions to products during the design phase.
Meanwhile, devices specifically designed to
reproduce effects, such as safety eyewear and helmets, can insert
computer-generated graphics into workers’ field of vision, which delivers real-time
assistance when they are performing their tasks.
These new technologies are still in their
teething stages when it comes to the manufacturing industry, but they are
growing fast and could have a major impact in 2020.
4th
solution: Keep your eyes open
The manufacturing industry is constantly
innovating, which is why it is so important to be attentive and anticipate any
changes shaping the industry of tomorrow.
To discover the other future trends for 2020, download the infographic entitled The new trends to watch in industry in 2020