Component manufacturers: three ways to generate leads through your website
To optimize your performance, you have decided to publish your component catalogs online in order to generate leads via the Internet. Are the results not as good as you expected? Below are three ideas to help you generate leads through your website as a component manufacturer.
1. Improve your natural referencing
This is an important initial point.
Search engine optimization (SEO) is crucial for generating leads through your website.
To improve your natural SEO, you must write content that is optimized for the web and that is specifically aimed at your prospects.
In other words, industrial buyers must feel you provide added value when they read your publications.
Your publications must be suited to search engines.
If Google considers that your content does not meet its quality standards, you will never be well positioned and therefore never visited by prospects.
To generate leads through your website, you have to improve your natural referencing (SEO) to appear on search engines.
This step takes time but leads to very good results in the long term.
2. Provide assistance to your visitors
The first step is ok. Visitors are on your site thanks to your good search engine optimization. So, what happens now?
If your answer is โnothingโ or โnot muchโ, the few lines that follow will certainly be of interest to you.
To generate leads through your website, you should not let your visitors leave too quickly.
In many cases, component manufacturers allow visitors to download the technical data of a component or to fill their shopping cart and purchase online.
However, your visitors are often at the stage where they want to compare products and need the help of an expert (or your companyโs expertise) to move towards a final purchasing decision.
In short, your visitors need help to make their purchasing decision.
Using a chat feature on your technical-presentation pages is a good way to provide your expert advice.
Your visitors need expert assistance, and thanks to this type of chat function you can provide the information they need when they need it most.
3. Encourage your visitors to fill out your contact forms
To generate leads, visitors to your web site must leave their contact details.
To achieve this, you must provide them with a contact form.
Note: there should be just one form which only proposes an initial contact.
As component manufacturers, you must provide several contact points on your website to increase the number of leads generated.
You have to propose premium content offers.
Premium content is downloadable content on your site that brings added value to your prospects.
For example, a computer-graphic presentation about industrial automation or a study about Industry 4.0 are subjects that will enable you to obtain contact details, and therefore leads, through your website.
Talk to one of our experts about how to generate leads through your website. Get a free audit now!
TraceParts is one of the worldโs leading CAD-content platforms for Engineering, Industrial Equipment and Machine Design. TraceParts brings highly targeted Lead Generation marketing services to hundreds of customers of all sizes and from all industries, via powerful cloud-based API and SaaS applications such as 3D part libraries, product catalogs and configurators.
Tipo: Plataforma de IA para projetistas mecรขnicos Alcance: 57.000 usuรกrios registrados
Leoโข รฉ a primeira IA do mundo feita para engenheiros mecรขnicos, ajudando mais de 57.000 engenheiros em empresas como HP, Scania e Intel a reduzir erros de projeto, aumentar a reutilizaรงรฃo de peรงas em um terรงo e economizar 12 horas de trabalho por engenheiro semanalmente. Alimentado por um Large Mechanical Model (LMM) proprietรกrio, Leo entende de forma รบnica arquivos CAD, especificaรงรตes e montagens, integra-se ao PLM para um contexto completo e oferece respostas com base nos seus dados ou em mais de um milhรฃo de fontes externas confiรกveis e mais de 100 milhรตes de peรงas padrรฃo para a mais alta precisรฃo. Com seguranรงa de nรญvel empresarial que garante que seus dados permaneรงam protegidos, Leo foi fundado em 2023 por especialistas do MIT, Technion, Microsoft e Elbit.
Leo AI
Tipo: Plataforma de IA para diseรฑadores mecรกnicos Alcance: 57.000 usuarios registrados
Leoโข es la primera IA del mundo creada especรญficamente para ingenieros mecรกnicos. Ya ayuda a mรกs de 57.000 ingenieros en todo el mundo โ en empresas como HP, Scania e Intel โ a reducir errores de diseรฑo, aumentar la reutilizaciรณn de piezas en un tercio y ahorrar hasta 12 horas de trabajo semanales por ingeniero.
Impulsado por un Large Mechanical Model (LMM) propio, Leo entiende de forma รบnica CAD, especificaciones y ensamblajes, se integra con sistemas PLM para ofrecer un contexto completo y proporciona respuestas basadas en sus propios datos o en mรกs de un millรณn de fuentes externas fiables y mรกs de 100 millones de piezas estรกndar, garantizando la mรกxima precisiรณn.
Con seguridad de nivel empresarial para proteger sus datos, Leo fue fundado en 2023 por expertos del MIT, Technion, Microsoft y Elbit.
Leoโข ist die weltweit erste KI, die speziell fรผr Maschinenbauingenieure entwickelt wurde. Sie unterstรผtzt bereits รผber 57.000 Ingenieure weltweit โ bei Unternehmen wie HP, Scania und Intel โ dabei, Konstruktionsfehler zu reduzieren, die Wiederverwendung von Teilen um ein Drittel zu steigern und jede Woche bis zu 12 Arbeitsstunden pro Ingenieur einzusparen.
Angetrieben von einem proprietรคren Large Mechanical Model (LMM) versteht Leo einzigartig CAD, Spezifikationen und Baugruppen, integriert sich in PLM-Systeme fรผr den vollstรคndigen Kontext und liefert Antworten, die entweder auf Ihren eigenen Daten oder auf mehr als einer Million vertrauenswรผrdiger externer Quellen und รผber 100 Millionen Normteilen basieren โ fรผr hรถchste Genauigkeit.
Mit Sicherheit auf Enterprise-Niveau, die Ihre Daten zuverlรคssig schรผtzt, wurde Leo 2023 von Experten des MIT, Technion, Microsoft und Elbit gegrรผndet.
Leo AI
Type : Plateforme IA pour concepteurs mรฉcaniques Audience : 57 000 utilisateurs inscrits
Leoโข est la premiรจre IA au monde conรงue spรฉcifiquement pour les ingรฉnieurs en mรฉcanique. Elle aide dรฉjร plus de 57 000 ingรฉnieurs ร travers le monde โ dans des entreprises comme HP, Scania et Intel โ ร rรฉduire les erreurs de conception, ร augmenter la rรฉutilisation des piรจces dโun tiers et ร gagner jusquโร 12 heures de travail par ingรฉnieur chaque semaine.
Propulsรฉ par un Large Mechanical Model (LMM) propriรฉtaire, Leo comprend de maniรจre unique la CAO, les spรฉcifications et les assemblages, sโintรจgre aux systรจmes PLM pour fournir un contexte complet et dรฉlivre des rรฉponses fondรฉes sur vos propres donnรฉes ou sur plus dโun million de sources externes fiables et plus de 100 millions de piรจces standard, garantissant une prรฉcision maximale.
Avec un niveau de sรฉcuritรฉ de type entreprise assurant la protection de vos donnรฉes, Leo a รฉtรฉ fondรฉ en 2023 par des experts du MIT, du Technion, de Microsoft et dโElbit.
Leo AI
Tipo: Piattaforma AI per progettisti meccanici Copertura: 57.000 utenti registrati
Leoโข รจ la prima IA al mondo creata appositamente per gli ingegneri meccanici. Supporta giร oltre 57.000 ingegneri in tutto il mondo โ in aziende come HP, Scania e Intel โ aiutandoli a ridurre gli errori di progettazione, ad aumentare del 30% il riutilizzo dei componenti e a risparmiare fino a 12 ore di lavoro settimanali per ingegnere.
Basato su un Large Mechanical Model (LMM) proprietario, Leo comprende in modo unico CAD, specifiche e assiemi, si integra con i sistemi PLM per fornire il contesto completo e fornisce risposte basate sui vostri dati oppure su oltre un milione di fonti esterne affidabili e piรน di 100 milioni di componenti standard, garantendo la massima precisione.
Con un livello di sicurezza enterprise-grade che assicura la protezione dei vostri dati, Leo รจ stato fondato nel 2023 da esperti provenienti da MIT, Technion, Microsoft ed Elbit.