Table of content
Products_XX tabs
โProduct_XXโ fields
| Field name | Status | Definition |
Product_ID | Required | Identifier that you use to identify a product in your system. Authorized characters are: โA-Zโ, โa-zโ, โ0-9โ, โ_โ, โ.โ All other characters, such as characters with accents or space, are not allowed. To group several part numbers together in the same product, repeat the same product ID for each line of each part number. For any one product, this value must be the same in each โProducts_xxโ tab, as it is used to group data between tabs. Examples: โPart_1โ, โEAC.010_120โ, โABC123โ |
Product_Name | Required | Defines a name for the product. The maximum number of characters for each product name is 255. Example: โHexagon socket head cap screw, DIN 912 (ref 527)โ |
Product_Short_Description | Optional | Used to enter a short description of the product. The maximum number of characters for each short description is 255. |
Product_Long_Description | Optional | Used to enter a more detailled description of the product. The maximum number of characters for each long description is 2000. |
Classification_Category_ID | Required | Identifier used for specifying a category in the classification. The list of authorized identifiers is defined in the โClassificationAdvancedTemplateโ Excel file, supplied with the archive file when you downloaded the empty template. Only the identifier of the category in which you classified your product is required (not the full path from the root). For any one product, this value must be the same in each โProducts_xxโ tab. |
Product_Large_Picture_ FileName | Optional | Supplies the name of the image file showing the product. The image must be supplied together with the completed XLS template. Recommended picture size is 460 x 340 pixels. Larger pictures will be resized. If not provided, TraceParts will try to extract a screenshot from the supplied CAD file. For any one product, this value must be the same in each โProducts_xxโ tab. Example: โLargeProductPicture1.gifโ |
The โProduct_IDโ you provided is stored in the TraceParts System.
When you provide a template with a โProduct_IDโ that doesnโt exist in the TraceParts Sytem, a new product is created in the TraceParts System.
If you then provide a second template with a โProduct_IDโ that already exists in the TraceParts System, the existing product is overwritten.
“Document” fields
| Field name | Status | Definition |
Product_Document_ FileName ( + “_” + document number) | Optional | Specifies the file name of any document linked to the product. The maximum number of characters for each file name is 100. The authorized file types are defined here. Documents must be supplied together with the completed XLS template. This information is linked to the information in the โProduct_Document_Titleโ field below. Examples: โCatalogue_Page.pdfโ, โPresentation.htmlโ |
Product_Document _Title ( + “_” + document number ) | Optional but recommended for each document declared in โProduct_Document_ FileNameโ | This information is linked to the information in the โProduct_Document_FileNameโ field above. It specifies the title to be displayed to the user, next to the link to the document, instead of the actual file name. The maximum number of characters for each document title is 255. Examples: โTechnical documentโ, โDatasheetโ |
Product_Document _URL ( + “_” + URL number ) | Optional | Specifies an URL that points to an online document linked to the product. This information is linked to the information in the โProduct_Document_URL_Titleโ field below. The protocol (http, https, etc.) is required in the URL. The maximum number of characters for each URL is 2000. Example: โ/help/fr/Main.htmโ |
Product_Document _URL_Title ( + “_” + URL number ) | Optional but recommended for each URL declared in โProduct_Document_ URLโ | This information is linked to the information in the โProduct_Document_URLโ field above. It specifies a title for the corresponding link, to be displayed to the user, instead of the actual URL. The maximum number of characters for each URL title is 255. Example: โTraceParts Online Helpโ |
Part_Number_ EShop_URL | Optional | Specifies an URL that points to an online E-shop linked to the product. This information is linked to the information in the โPart_Number_EShop_URL_DisplayedValueโ field below. The protocol (http, https, etc.) is required in the URL. The maximum number of characters for each URL is 2000. The “Request for quotation” tab on www.traceparts.com is replaced by a new tab “Buy now”. |
Part_Number_ EShop_URL _DisplayedValue | Optional but recommended for each URL declared in โPart_Number_ EShop_URLโ | This information is linked to the information in the โPart_Number_EShop_URLโ field above. It specifies a title for the corresponding link, to be displayed to the user, instead of the actual URL. The maximum number of characters for each URL title is 255. |
Product_Dimensional_ Drawing_FileName ( + “_” + dimensional drawing number ) | Optional | Specifies the file name of the dimensional drawing linked to the product. The maximum number of characters for each file name is 100. This information is linked to the information in the โProduct_Dimensional_Drawing_Titleโ field below. Files must be supplied together with the completed XLS template. The authorized file types are picture formats (.gif, .png, .jpg, .bmp). Example: โFront_View.gifโ, โtech_doc_1.pngโ |
Product_Dimensional_ Drawing_Title ( + “_” + dimensional drawing number ) | Optional but recommended for each dimensional drawing declared in โProduct_ Dimensional_ Drawing_FileNameโ | This information is linked to the information in the โProduct_Dimensional_Drawing_FileNameโ field above. It specifies a title for the corresponding drawing, to be displayed to the user, instead of the actual file name. The maximum number of characters for each drawing title is 255. Example: โFront Viewโ, โDrawingโ |
The list of authorized external document types is as follows
“Part Number” fields
| Field name | Status | Definition |
Part_Number_Sort_ID | Required if you define some part numbers in โPart_Numberโ field | Numerical value starting from 1 to N for each product in order to make the part number record distinct for each product. For any one part number, this value must be the same in each โProducts_xxโ tab. |
Manufacturer_Name | Optional. | Allow to overwrite the name of the manufacturer defined at the catalog level. |
Distributor_ Part_Number | Optional. | Specify a Distributor part number. |
Distributor_Name | Optional. | Specify a Distributor name. |
Manufacturer_ Part_Number | Required if you define a CAD model, a description, or any attribute value (see โCustomizing the templateโ) | Define the part number. One part number per line. The maximum number of characters for each part number is 255. For any one Product_ID + Part_Number_ID pairing, this value must be the same in each โProducts_xxโ tab. |
Part_Number_ CAD_FileName | Optional | Defines the CAD file name to be used as the source 3D model. The maximum number of characters for each file name is 100. The file must be supplied together with the completed XLS template. For any one part number, this value must be the same in each โProducts_xxโ tab. For CAD assembly, create an archive file with all necessary files. The archive file name must be: MainCADFileName.CADExtension.archiveExtension. In the XLS template, enter the archive file name in the relevant field. Example, for a SolidWorks Assembly zip file: MyAssembly.sldasm.zip |
Part_Number _Description | Required if you define some part numbers in โPart_Numberโ field | Provides a description of the part number. The maximum number of characters for each description is 255. |
When you want to group several part numbers together in the same product, all data relating to the โProductโ and โDocumentโ fields must be duplicated with the same values for each part number line.
The list of supported CAD formats is as follows
“Attributes_Definition” tab
This tab contains information for customizing the template.
See the โCustomizing the templateโ section for more details.
| Field name | Status | Definition |
Attribute_ID | Required | Contains the list of attributes you have added to the template (see โCustomizing the templateโ). Remember that the items in this list are treated as the identifiers of the attributes. Therefore:
Examples: โDIAโ, โL0โ, โh1โ, โATT_1โ, โATT_2โ, โMATโ |
Attribute_ Name ( + “_” + language code ) | Required | Used to define the name for each of your attributes in the various languages selected (see โCustomizing the templateโ). This name is displayed to the user. If the values of your attribute are expressed in a specific unit, we recommend that you add the unit symbol at the end of the label. Examples: โInternal diameter (mm)โ, โL0 (mm)โ, โh1 (mm)โ, โTemperature (ยฐC)โ, โColorโ, โMaterialโ |
“System” tab
This tab contains information required by the programs that will be processing your data. It contains the answers to certain questions asked by the wizard.
Please do not make any change in the tab.
Fields defined in the โSystemโ tab
| Field name | Status | Definition |
System_ Attribute_Name | Required | (Reserved) Specifies a โsystemโ attribute used by the programs that will be processing the template file. See the list of system attributes. |
System_ Attribute_Value | Required | (Reserved) Value of a system attribute. |
List of system attributes
| System attribute name | System attribute value |
Template_Name | Template name. Predefined system value : “Self-Publishing Products Catalog” |
Template_Type | Template type. Predefined system value : “Basic Template” |
Template_Version | Template version. Predefined system value. |
Product_Document_Number | Number of the document selected by the user in the wizard (macro). |
Product_URL_Number | Number of the online document selected by the user in the wizard (macro). |
Product_Dimensional_Drawing_Number | Number of the dimensional drawing selected by the user in the wizard (macro). |
Default_Language_Code | Code of the default language selected by the user in the wizard (macro). |
Selected_Language_Code | Code of the language selected by the user in the wizard (macro). There may be one or more lines. Each line contains a single language code. |
Sample parts file, with English as selected language.
(splited in 4 parts due to the number of columns to display)
Startup: using the wizard > File structure > Customizing the template

Deutsch
Franรงais
Italiano
Espaรฑol
Portuguรชs
ไธญๆ (ไธญๅฝ)
ๆฅๆฌ่ช
ะ ัััะบะธะน